Device Address for PCA9955

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Device Address for PCA9955

3,296 次查看
philma
Contributor I

Hey there,

I'm trying to set up the PCA9955 Led Driver with I2C. I set the four hardware selectable pins A0-A3 to ground (VSS), so that the device adress should be 110 0000 (C0h including R/W bit). Problem is, the driver doesn't send an acknowledge bit as a response (I connected the I2C to an oscilloscope).

By addressing it with the ALLCALLADR (E0h) or SUBADDRESS (ECh) an acknowledge bit is set und the following messages can be transmitted.

As I got only one driver on the bus I could use this addresses to set up the driver, but as I read in the datasheet, this address is only for read transactions?

I can't get the issue of the addressing problem. The selected address shouldn't be a permitted one...

Hope someone can help.

Greeting,
Phil

0 项奖励
回复
3 回复数

3,066 次查看
david_diaz
NXP Employee
NXP Employee

Hello Phil,

The I2C-bus slave address of the PCA9955B is shown in Figure 3 from datasheet. The 7-bit slave address is determined by the quinary input pads AD0, AD1 and AD2.

When the input pins are connected to ground, the I2C address is 0000001 based on the Table 5 below:

pastedImage_1.png

Can you please verity your input pins connection?

Regards,

David

3,066 次查看
tomasreabe
Contributor I

Yes I did an PR for the PCA 9955 but purchasing got the PCA9955B as that is what is now out there.

So the address is working as it should but I now have the problem of being on address 5 as that is a reserved address for high speed I2C. Time for a PCB redesign and Fix.

0 项奖励
回复

3,066 次查看
tomasreabe
Contributor I

I have 5 of these chips on a PCB and one other chip on the I2C bus

I do get a Ack from the other chip on the bus a PCA 9555 at 0100 000

but none of the PCA 9955 chips are giving ack on the addresses expected for direct addressing.

I do get responses at these address

0000 000

0000 001

0000 101

0010 101

0011 010

1100 101

1110 000

1110 110

I should be getting responses at

0000 000

1100 000

1100 001

1100 010

1100 011

1100 100

1110 000

1110 110

0 项奖励
回复