Demo application of voice control gui application gets stuck in im8MPlus flashed with LInuxBSP6.5.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Demo application of voice control gui application gets stuck in im8MPlus flashed with LInuxBSP6.5.2

513 次查看
PoojaSk
Contributor II

Hi,

Tried running the gopoint voice control applicaton wakeword_demo  in imx8mplus flashed with linuxBSP the gui is stuck after launching. This is the case for all the applications, but running the face recognition application without gui works fine. So how can I run the voicecontrol application  which wakes the board with "Hey NXP" without gui. where can I get the model files for the same. If ready script is not available as I could see the model files are hardcoded with the gui app.

Thanks,
Pooja

0 项奖励
回复
3 回复数

490 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @PoojaSk!

Thank you for contacting NXP Support!

 

What board are you using?

Are you using the BSP 6.6.52?

 

That example is running in our IMX93-EVK board but no in iMX8MP-EVK board due to the IMX8MP-EVK board does not have microphones.

0 项奖励
回复

475 次查看
PoojaSk
Contributor II

Hi @Chavira 

So I have Imx8MPlus board flashed with Linux BSP 6.6.52. I am Unable to run any of the (not just audio related) Gopoint applications as the GUI is stuck after launching app. Also my requirement was to execute a wake word detection in the board by using the microphone of connected headset which is able to record audio. So are these go point applications exclusively for IMX93? Also will moving to IMX93 makes it possible to use wake word detector demo?

Thanks,
Pooja

标记 (1)
0 项奖励
回复

461 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @PoojaSk!

 

This demo is working in the iMX93-EVK ate the moment:

 

Chavira_0-1746188569767.png

 

0 项奖励
回复