Demo application of voice control gui application gets stuck in im8MPlus flashed with LInuxBSP6.5.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Demo application of voice control gui application gets stuck in im8MPlus flashed with LInuxBSP6.5.2

514 Views
PoojaSk
Contributor II

Hi,

Tried running the gopoint voice control applicaton wakeword_demo  in imx8mplus flashed with linuxBSP the gui is stuck after launching. This is the case for all the applications, but running the face recognition application without gui works fine. So how can I run the voicecontrol application  which wakes the board with "Hey NXP" without gui. where can I get the model files for the same. If ready script is not available as I could see the model files are hardcoded with the gui app.

Thanks,
Pooja

0 Kudos
Reply
3 Replies

491 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @PoojaSk!

Thank you for contacting NXP Support!

 

What board are you using?

Are you using the BSP 6.6.52?

 

That example is running in our IMX93-EVK board but no in iMX8MP-EVK board due to the IMX8MP-EVK board does not have microphones.

0 Kudos
Reply

476 Views
PoojaSk
Contributor II

Hi @Chavira 

So I have Imx8MPlus board flashed with Linux BSP 6.6.52. I am Unable to run any of the (not just audio related) Gopoint applications as the GUI is stuck after launching app. Also my requirement was to execute a wake word detection in the board by using the microphone of connected headset which is able to record audio. So are these go point applications exclusively for IMX93? Also will moving to IMX93 makes it possible to use wake word detector demo?

Thanks,
Pooja

Tags (1)
0 Kudos
Reply

462 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @PoojaSk!

 

This demo is working in the iMX93-EVK ate the moment:

 

Chavira_0-1746188569767.png

 

0 Kudos
Reply