Debuge Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debuge Issue

1,666 Views
shrikant_koli
Contributor I

i have MKW38A512VFT4 NXP microcontroller in actual hardware board. into that we are upload the driver code using SEGGER j-link debugger ; but its not debuggable. 

its stuck into the startup file.

shrikant_koli_0-1633064701665.png

 

below are the debugger setting.

shrikant_koli_1-1633064826873.pngshrikant_koli_2-1633064866841.pngshrikant_koli_3-1633064902902.pngshrikant_koli_4-1633064921312.pngshrikant_koli_5-1633064938400.pngshrikant_koli_6-1633064958960.pngshrikant_koli_7-1633064972620.pngshrikant_koli_8-1633064994865.pngshrikant_koli_9-1633065007073.png

Debugging purpose we are use below schematic.

shrikant_koli_10-1633065147927.png

 

if i have use FRDM-KW38 devlopment board then its has debuge.

So is their any setting for debugging the driver code into actual hardware.

please suggest me.

0 Kudos
Reply
2 Replies

1,634 Views
shrikant_koli
Contributor I

Hello Sir,

Thanks for your suggestion.

Yes , we are reffering custom designed board.

we forget to pull-up PTB18.

After pull-up that pin . i am able to debug driver code into custom designed board.

Once again thank you so much.

 

 

 

 

0 Kudos
Reply

1,638 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. With actual hardware board, are you referring that is your custom designed board?

You are getting stuck in the NMI_Handler. Could you please clarify if you have a pull-up resistor in that pin? (PTB18)

 

Best Regards,

Ricardo

0 Kudos
Reply