Debug Issue in IMXRT1170-EVKB with MCUXpresso_IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Issue in IMXRT1170-EVKB with MCUXpresso_IDE

498 次查看
Shivani_Elavena
Contributor II

Hii,

When I am trying to debug the imported example of IMXRT1170-EVKB IN MCUXpresso-IDE, it is not going into the debug and getting an error. Only once it went into the debug correctly, after that it is throughing errors. And I also attaching a file of the debug issue shown in the IDE.

I've connected power cable to the J43 and USB (debug) to the J86 and SW5 is in ON Position.

Thank you...

0 项奖励
回复
1 回复

479 次查看
mayliu1
NXP Employee
NXP Employee

Hi @Shivani_Elavena ,

Thank you so much for your interest in our products and for using our community.

First, I advice you check J38 setting. If you use power cable to the J43, J38 Pin1 should connect Pin2.

Fig1.png

Second, Please check your BOOT_CFG and  BOOT_MODE configuration.

Normally, If you do not modify your MIMXRT1170-EVKB board, Please set SW2 all 0, Set SW1:0010(Internal Boot).

 

Fig2.png

 

Please check, If you still have problem, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

0 项奖励
回复