DSP56321 Longevity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,982件の閲覧回数
ThomasFunk
Contributor I

Hi There,

 

Can someone indicate what the longevity "plan" is/was for the DSP56321 especially the DSP56321VL275.

What was the launch date, does it have an extended longevity of 15, 20 or 25 years and until when it will stay in the longevity "plan"?

0 件の賞賛
返信
1 解決策
2,976件の閲覧回数
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Thomas,

DSP56321 has been launched in Feb 2005 and the lifetime is guaranteed 10years, as you can easily check in NXP Product Longevity Program:

https://www.nxp.com/products/product-information/product-programs/product-longevity:PRDCT_LONGEVITY_...

Please note that it does not necessarily mean EOL (End of Life). It means that rest of the product life depends on customers' demand.

Have a nice day.

Pavla 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,977件の閲覧回数
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Thomas,

DSP56321 has been launched in Feb 2005 and the lifetime is guaranteed 10years, as you can easily check in NXP Product Longevity Program:

https://www.nxp.com/products/product-information/product-programs/product-longevity:PRDCT_LONGEVITY_...

Please note that it does not necessarily mean EOL (End of Life). It means that rest of the product life depends on customers' demand.

Have a nice day.

Pavla 

0 件の賞賛
返信
2,721件の閲覧回数
ThomasFunk
Contributor I

Hi,

I noticed the status for the DSP56321VL275 shows now End-of-Life, but there is no last-time-buy date published. Is the status the same as in May 2022 or did the status change since May 2022 ?

Can I still purchase 3 trays from NXP? (i.e 378 devices)

Looking forward to your reply.

0 件の賞賛
返信