DDR2 data lines not being driven in write cycle (MPC8377)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR2 data lines not being driven in write cycle (MPC8377)

ソリューションへジャンプ
3,201件の閲覧回数
mvonahnen
Contributor II
Has anybody seen an issue where the MQxx data lines do not drive the bus in a write cycle?  We have a new board we have designed.

We are using 64 bit bus,  using 4x MT47H64M16HR-3IT memory chips from Micron.  We have tried running the DDR2 at a slow speed just to verify operation, so we have configured it for a 133 MHz clock rate.  We are seeing all of the control signals and captured a write cycle with our oscope / logic analyzer.  Every thing looks good, except for the data lines do not appear to drive.  When ODT is enabled, the data lines are at 0.9 V while MDQS is toggling.

We suspect pretty much everything in the design, but we have verified the following things:

1.  All of the 1.8 V supply pins have power.
2.  The processor is getting clocks.
3.  The output DDR2 clocks are what are expected.

We are configuring the reset configuration words from the CodeWarrior USB TAP. 

I have attached our measurement.  Note, the CS# / Clock relationship shown by the logic analyzer traces does not represent the actual timing.

Any suggestions on things to go look at?

atlas_wr_all_ones.jpg
Message Edited by t.dowe on 2009-10-20 01:03 PM
0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
mvonahnen
Contributor II
Some additional information.  All 8 MDQS and MDM signals are driven for access, even if we are doing byte level accesses.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,822件の閲覧回数
mvonahnen
Contributor II
Some additional information.  All 8 MDQS and MDM signals are driven for access, even if we are doing byte level accesses.
0 件の賞賛
返信
1,821件の閲覧回数
mvonahnen
Contributor II
The problem was found, a pull down was mistakenly placed on CFG_LYNX_TEST (which shares a pin with USB1_STP).  This caused the part to go into a partial test mode.  Removing the pull down fixed the issue.
0 件の賞賛
返信