Could not resolve host: source.codeaurora.cn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could not resolve host: source.codeaurora.cn

5,110件の閲覧回数
kangqin
Contributor I

In the Android build step, in imx-p9.0.0_ 2.1.0 Execute source envsetup.sh in the auto-ga file path, and an error occurred: Could not resolve host: source.codeaurora.cn   ,How can I make envsetup.sh successful?

0 件の賞賛
返信
4 返答(返信)

5,081件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Please mention the steps you are following to reproduce the issue at our end.
Kindly attach the whole error logs you are getting for further debugging the issue.
 
Thanks & Regards
Sanket Parekh
0 件の賞賛
返信

5,069件の閲覧回数
kangqin
Contributor I

Thank you for your reply~

As shown in the figure, this is the step I took   

Follow the steps of “Android_User's_Guide.pdf”

0 件の賞賛
返信

5,065件の閲覧回数
kangqin
Contributor I

/imx$ source ./imx-p9.0.0_2.1.0-auto-ga/imx_android_setup.sh
Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/root123/imx/imx-p9.0.0_2.1.0-auto-ga
Downloading Repo source from https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/
remote: Enumerating objects: 4483, done.
remote: Counting objects: 100% (4483/4483), done.
remote: Compressing objects: 100% (2133/2133), done.
remote: Total 8049 (delta 3993), reused 2350 (delta 2350), pack-reused 3566
Receiving objects: 100% (8049/8049), 3.79 MiB | 9.92 MiB/s, done.
Resolving deltas: 100% (5176/5176), done.

manifests:
fatal: unable to access 'http://source.codeaurora.cn/external/imx/imx-manifest.git/': Could not resolve host: source.codeaurora.cn
manifests: sleeping 4.0 seconds before retrying

manifests:
fatal: unable to access 'http://source.codeaurora.cn/external/imx/imx-manifest.git/': Could not resolve host: source.codeaurora.cn
fatal: cannot obtain manifest https://source.codeaurora.org/external/imx/imx-manifest.git
---------------------------------------------------
-----Repo Init failure
---------------------------------------------------

0 件の賞賛
返信

4,979件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @kangqin 
 
I hope you are doing well
 

 

The steps seem correct. Kindly confirm that you are downloading the source code from the below official link.

 

 
Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信