Controlling MC33772C via direct SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Controlling MC33772C via direct SPI

1,141件の閲覧回数
hbsantos
Contributor II

I need to control the mc33772c via the s32k344 SPI, but I'm using the Bms_common SDK library with mc33665A and mc33775a. is it possible to create a second instance of bms_common to control the mc33772c? Or is there another possibility of configuration via direct SPI communication with the mc33772c?

 

hbsantos_0-1706016650998.png

タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,114件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If you don't need TPL communication you can directly build the SPI communication between MC3377X and MCU:

guoweisun_0-1706233892220.png

 

0 件の賞賛
返信

1,073件の閲覧回数
hbsantos
Contributor II

Ok, but I would like to use the BMS SDK, is it possible? Because the MC33772C driver is not compatible with S32K3 micrcontrollers.

タグ(2)
0 件の賞賛
返信