Controller selection for CLRC663

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Controller selection for CLRC663

1,206件の閲覧回数
chand_padaliya
Contributor I

Hi,
i am new in RFID Based product designing.

in my application i want to use mi-fare classic card for authentication purpose.

i have gone through development schematics and found LPC1769 controller was used as a host controller.

my question is can i use oher controller instead of LPC1769?

which are the selection criteria to use another controller?

as used LPC1769 has more pin count with larger size.

 

0 件の賞賛
返信
1 返信

1,188件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. The CLRC663 is a frontend that works command based, so you can send the SPI commands with your host MCU. We recommend to use the NFC Reader Library.

 

We have some guides you help you in the migration process, the first thing I would recommend you to check would be the NFC Reader Library webinar to understand the structure of the library.

 

Once you have understand it, you can check the following guides for the migration process.

Porting NFC Reader Library to Kinetis K64 | Document | Video

Porting NFC Reader Library to LPC11u37h | Document I, II, III, IV

Porting NFC Reader Library to i.MX RT1050  | Document | Video

 

Also you can check  the AN11908, please consider the memory requirements to deploy the library in your device as well as the protocol necessities regarding the clocks of the device and do not forget to read the license agreement of the library.

 

Best Regards,

Ricardo

0 件の賞賛
返信