OCXO can be used as external clock reference with TFF1024HN. Application note AN11516 describes using external crystal oscillator circuit based on 74LVC1GU04. It also describes requirements for XO1/XO2 signals which should the circuit provide.
In this application note, GU04 inverter provides differential output (180 degree phase shift), passive RC networks scale the amplitude and to match output impedances. You can follow the circuit in Figure 17 or make your own circuit for a design that gets a clock from external source (OCXO).
Note, poor layout may cause excessive phase noise and jitter. All the suggestions from Section 4.1 are applicable.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------