Configtool SJA1110 scripting/ command line interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configtool SJA1110 scripting/ command line interface

1,871 次查看
lorenzo_giraudi
Contributor III

Hello,

I am working on a project where I have two SJA1110 that are almost the same apart from some L2 Look-up Table entries. 

The issue is that the only way that I know to modify the L2 entry is through the ConfigTool, which:

  • at least on my pc is really slow
  • cannot be scripted
  • cannot use macros/define of the C code

This makes S32DS really limiting since the GUI is not flexible enough. I would like to avoid having two projects and having to replicate the changes by hand through the GUI... this is really error-prone.

Are there are any other ways?

Thank you!

标记 (3)
0 项奖励
回复
1 回复

1,839 次查看
bpe
NXP Employee
NXP Employee

You are asking about a preproduction device. Currently, all documentation and software for it are available under NDA. For this reason, the only information I can share in a public Forum is, that there are script-based tools to generate static switch configuration files. If your company/organization has a valid NDA with NXP, please open a Support Case to receive more suggestions.

Best Regards,
Platon

 

 

0 项奖励
回复