Codewarrior P2020 AN4039-DDR3调试工具问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior P2020 AN4039-DDR3调试工具问题

2,089 Views
wangrui_202077
Contributor I

Hi:

       我这边需要用Codewarrior 连接P2020来调试 AN4039-DDR3参数,论坛上看到Codewarrior 有DDR相关调试工具手册QCVS_DDR_User_Guide.pdf,想问下Codewarrior10.1.1或10.5.1里面自带DDR QCVS工具吗?还是需另外下载相关工具?另外通过Codewarrior快速调试DDR3参数的工具和方法有哪些?请帮忙赐教下,非常感谢。

 

0 Kudos
Reply
4 Replies

2,087 Views
wangrui_202077
Contributor I

QCS DDRV SW tool 帮忙提供下该工具下载链接。

0 Kudos
Reply

2,081 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could download QCVS for PowerPC from the following link.

链接: https://pan.baidu.com/s/1G5U8T721B7pJigtZbDP0oQ

提取码: rev1

Please install QCVS package from Help->Install New Software->Add->Archive.

 

Use the tool to generate the DDR register settings

Select the SPD option in configuration wizard when DIMM is used

Select Auto Configuration when Discrete DRAM is used

 

 

0 Kudos
Reply

1,504 Views
18016209476
Contributor I

可以重新分享一份吗,谢谢~

0 Kudos
Reply

1,618 Views
starto
Contributor II

百度网盘链接已经失效,能否重新发一份?

0 Kudos
Reply