Code source fo internal clock for NXP S32K146

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code source fo internal clock for NXP S32K146

1,514 Views
sebastien_ledio
Contributor I

Hello,

I am developping SW on S32K146 NXP microprocessor. Actually I use an external cristal for system clock. The SW runs correctly.

Now, I would like to remove this cristal, so use the internal clock, but something does not work.

Someone can help me by give me an source code example to know how configure internal clock without cristal.

By advance, thanks a lot

0 Kudos
Reply
1 Reply

1,467 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Sebastien Le Diouris

The default configuration out of reset has the CPU clocked by the Fast IRC (FIRC_CLK), so actually, you should be able to run the MCU without an external crystal. are you setting up the external clock in your startup file? could you clarify what part doesn't work, or what behaviour are you seeing?


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply