Cd1030: Linux kernel driver required

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cd1030: Linux kernel driver required

1,389件の閲覧回数
DhavalS
Contributor II

We are using the i.mx8qm processor.

 

CD1030 is interfaced with i.mx8qm over lpspi1 interface.

 

I cann't see any linux kernel driver of the cd1030 nxp chipset in latest linux kernel.

I get one referance of RTOS based code but no linux kernel driver for this chipset.

 

Can you please provide the linux kernel driver for this NXP CD1030 driver?

 

I have used the generic spidev driver to check but that is not working

dts file changes

&lpspi1 {

compatible = "fsl,imx8qm-lpspi", "fsl,imx7ulp-spi";
#address-cells = <1>;
#size-cells = <0>;
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi1 &pinctrl_lpspi1_cs>;
cs-gpios = <&lsio_gpio3 24 GPIO_ACTIVE_LOW>;
status = "okay";

spidev0: spi@0 { //Digital Input
reg = <0>;
compatible = "rohm,dh2228fv";
spi-max-frequency = <30000000>;
};
};

pinctrl_lpspi1: lpspi1grp {
fsl,pins = <
IMX8QM_ADC_IN3_DMA_SPI1_SCK 0x06000040
IMX8QM_ADC_IN4_DMA_SPI1_SDO 0x06000040
IMX8QM_ADC_IN5_DMA_SPI1_SDI 0x06000040
IMX8QM_LVDS1_I2C0_SDA_LSIO_GPIO1_IO13 0x06000020
>;
};

pinctrl_lpspi1_cs: lpspi1cs {
fsl,pins = <
IMX8QM_ADC_IN6_LSIO_GPIO3_IO24 0x21
>;
};

 I can see that /dev/spidev0.0 node is created and when try to test using the loopback test don't see the response back (MOSI and MISO  are Shorted)

root@dictgu:~# spidev_test -v -D /dev/spidev0.0
spi mode: 0x0
bits per word: 8
max speed: 500000 Hz (500 kHz)
TX | FF FF FF FF FF FF 40 00 00 00 00 95 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF F0 0D |......@.........................|
RX | 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................................|

 

Is this driver should work?

 

If no then please provide the linux kernel driver for CD1030

タグ(3)
0 件の賞賛
返信
1 返信

1,377件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dhaval 

 

nxp provides drivers only for peripheral chips present in nxp reference boards (Sabre SD, EVK,

MEK). For other peripherals drivers may be obtained using support of  https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 件の賞賛
返信