I use CLRC663 as NFC frontend IC and the NTAG210_NTAG212 (NTAG210 used IC in Murata Tag LXMS33HCNK-171) as target.
I use the CLRC663 without library according to application note AN12657 and use a custom board.
The detection of the tag works reliable but from time to time (error quote is 5 - 10 %) the CLRC663 cancels my ISO14443 write command due to timeout which is caused by not setting the RxIRQ bit in IRQ0 register. The error register shows me that a Min
FrameErr (error bit 0x10) has occured. What causes this error?
In case that my rf field modulation is not strong enough I would assume a higher error quote of > 50 %. The command itself must be correct, because in most cases It works as expected.
Are there any additional settings which influence this behaviour?
Kind regards
Sascha