Cascading 74LVC595A shift registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cascading 74LVC595A shift registers

1,525 Views
franzforstmayr
Contributor I

Hey,
the 74LVC595A shift registers reads the incoming data with the rising clock edge. The serial data output is also clocked on the rising edge of the SHCP. Could there be a problem when cascading several 74LVC595A devices, due to propagation delay and  hold time? I mean the cascaded register has a hold time of minimum 1.5ns at 3.3V, the data output could have a propagation delay of 1.5ns. This means the second register can see a changing input pin 1.5ns after the clock pulse, so layout effects of a few ps can make my device unfunctional by reading strange things.

Is there a good way to avoid problems like this? Why isn't a additional Q7S flip flop in the device, which latches the data out at the falling clock edge?

Yours Franz

Tags (2)
0 Kudos
Reply
1 Reply

1,399 Views
Bulat
NXP Employee
NXP Employee

It should not be a problem, everything will work correctly as you expect.
If you are going to work at very high clock frequencies, there is a reason to pay attention to clock routing. Specifically, clock delay from the clock source to clock inputs of all shift registers should be the same.

Regards,

Bulat