Camera input format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera input format

1,320 Views
Kuntalaman
Contributor II

Hello i selected RT1170 MCU for my image capturing project, today in the market each camera sensor support RAW format and "the RT1170 is designed to support 24-bit RGB888/YUV444,
CCIR656 video interface, 8-bit YCbCr, YUV or RGB,and 8-bit/10-bit/16-bit/24-bit Bayer data input. " i only want to capture the photograph, please clarify what type of format it it will support will it be able to support RAW data if not then what data it will support please clear it

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

1,289 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Kuntalaman ,

Thanks for your interest in NXP MIMXRT series!

MIPI-CSI2 support the following RGB formats(RGB444, RGB555, RGB565, RGB666, RGB888) , MJPEG. But it doesn't support: Raw data(both raw8, raw10) and YUV422(10 bit).

CSI Parallel Camera can support:
• 8-bit / 16-bit / 24-bit data port for YCbCr, YUV, or RGB data input.
• 8-bit / 10-bit / 16-bit data port for Bayer data input.

Best regards,
Gavin

0 Kudos
Reply