CLRC663 Rx pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 Rx pin

2,267 Views
muratt
Contributor I

Hello,

Currently ı have a design which ı am using #MFRC522. Right now ı am updating this design for #CLRC663 plus. I have question about that:

Why there are two Tx pin İn both IC?

Why #MFRC522 has one Rx pin and#CLRC663 has two?

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
4 Replies

2,223 Views
muratt
Contributor I

Thanks for your answer. what is the reason of two tx and one tvss pins for antenna?

0 Kudos
Reply

2,243 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @muratt 

This is determined by the internal structure of the IC. CLRC663 adds a mixer to optimize the RX performance, is backward compatible with MFRC522, and has various performance improvements.

 

KellyLi_0-1735207917549.png

 

0 Kudos
Reply

2,252 Views
muratt
Contributor I

And is there any specification about how can ı learn the reading distance?

0 Kudos
Reply

2,241 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @muratt 

Reading distance depends on the antenna design, so it's recommended that you can refer to AN11019

https://www.nxp.com/docs/en/application-note/AN11019.pdf

0 Kudos
Reply