CLRC663 Rx pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLRC663 Rx pin

2,314 次查看
muratt
Contributor I

Hello,

Currently ı have a design which ı am using #MFRC522. Right now ı am updating this design for #CLRC663 plus. I have question about that:

Why there are two Tx pin İn both IC?

Why #MFRC522 has one Rx pin and#CLRC663 has two?

标签 (1)
  • RF

标记 (1)
0 项奖励
回复
4 回复数

2,270 次查看
muratt
Contributor I

Thanks for your answer. what is the reason of two tx and one tvss pins for antenna?

0 项奖励
回复

2,290 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @muratt 

This is determined by the internal structure of the IC. CLRC663 adds a mixer to optimize the RX performance, is backward compatible with MFRC522, and has various performance improvements.

 

KellyLi_0-1735207917549.png

 

0 项奖励
回复

2,299 次查看
muratt
Contributor I

And is there any specification about how can ı learn the reading distance?

0 项奖励
回复

2,288 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @muratt 

Reading distance depends on the antenna design, so it's recommended that you can refer to AN11019

https://www.nxp.com/docs/en/application-note/AN11019.pdf

0 项奖励
回复