CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command

2,419 Views
software_memo
Contributor II

Hi,

Can anyone please provide some guidance for settings up the registers in either the CLRC632 or SLRC400 to send an inventory command to ISO15693 compliant cards? Any application notes or example code would be very much appreciated.

Thanks,

Luke

0 Kudos
Reply
3 Replies

2,416 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @software_memo ,

 

There is a script file available for this purpose, please kindly refer to https://www.nxp.com/downloads/en/software/210910.zip for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,412 Views
software_memo
Contributor II

Hi,

Thank you so much for quick response however the scripts you mentioned are for the new CLRC663 product family range.

Do you have something similar for the older version of these ICs namely the SLRc400 and CLRC632? 

Thanks,

Luke

0 Kudos
Reply

2,405 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @software_memo ,

 

I am sorry but no such kind of example available, we recommend CLRC663 plus for new design.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply