CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command

2,433 次查看
software_memo
Contributor II

Hi,

Can anyone please provide some guidance for settings up the registers in either the CLRC632 or SLRC400 to send an inventory command to ISO15693 compliant cards? Any application notes or example code would be very much appreciated.

Thanks,

Luke

0 项奖励
回复
3 回复数

2,430 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @software_memo ,

 

There is a script file available for this purpose, please kindly refer to https://www.nxp.com/downloads/en/software/210910.zip for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,426 次查看
software_memo
Contributor II

Hi,

Thank you so much for quick response however the scripts you mentioned are for the new CLRC663 product family range.

Do you have something similar for the older version of these ICs namely the SLRc400 and CLRC632? 

Thanks,

Luke

0 项奖励
回复

2,419 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @software_memo ,

 

I am sorry but no such kind of example available, we recommend CLRC663 plus for new design.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复