Bootloader code for the MPC5604

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader code for the MPC5604

4,860件の閲覧回数
bryanwade
Contributor I

I'm just getting started Freescale products so please forgive me if I'm missing something obvious. Is there any example bootloader code available for the the MPC5604P or similar?

Ultimately I plan to update application code via Flexray, but a UART or CAN example would be a good starting point.

Thanks.

3 返答(返信)

3,250件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached you will find draft of my application note. Hope it will be useful.

Lukas

3,250件の閲覧回数
Stevanatto
Contributor II

I will use this code too. Thank you.

0 件の賞賛
返信

3,250件の閲覧回数
gangzhou
Contributor II

Tkank you for sharing the bootloader code.I want to write a bootloader for MPC5644A according to your code.But,the program can not run properly.And ,stop at function EXCEP_DefaultExceptionHandler().Whether I must write some command files in my project like

"t32" file  in your project or not? How should I do?

0 件の賞賛
返信