Bootloader Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader Code

2,601件の閲覧回数
Abhisek20
Contributor I

Hi,

I am using SDK bootloader example(evkbmimxrt1170_flashloader_cm7) for flashing new firmware into evkbmimxrt1170. I am new to this controller. Can you please give me some kind of documentation for this sdk example project or some kind of explanation of what this code basically does?

 

Regards

Abhisek

0 件の賞賛
返信
4 返答(返信)

2,413件の閲覧回数
Abhisek20
Contributor I

Hi Gavin,

Thanks for your inputs.

 

0 件の賞賛
返信

2,573件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Abhisek20 ,

Thanks for your interest in NXP MIMXRT series!

Flashloader provides a way to download the Application into all external non-volatile memories supported by i.MXRT1xxx to prepare for subsequent booting from external memories. It can be a perfect complement to BootROM, and at the same time, there are customers who use it as a secondary bootloader to update their own images without having to develop their own bootloader and host PC software. 

You can refer to this AN: https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

Also, there are two very good Chinese documents that provide detailed development steps that might help you as well:
1. https://www.cnblogs.com/henjay724/p/9098577.html
2. https://www.nxpic.org.cn/module/forum/thread-620172-1-1.html

Best regards,
Gavin

0 件の賞賛
返信

2,482件の閲覧回数
Abhisek20
Contributor I

Hi,

I tried to send the application binary using UART1 through Tera Term. But still I am not able to update the firmware. If you can provide me with me steps on how to send the application binary and what type of file format it is expecting, so that we will be able to upgrade the firmware.

regards

abhisek

0 件の賞賛
返信

2,469件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Abhisek20 ,

Thanks for your feedback.

There are two more important concepts that I hope we can explain first:

1. First of all, the flashloader project is running in RAM;

2. If you need to put the image to be updated into flash, you have to configure external storage, which will run a bunch of blhost commands;

3. If we don't have a flashloader project and need to use blhost, then we can only change SW1 into serial download mode to do the work afterward.

Based on the above, we skipped step 3 by running the flashloader project in RAM first. Then, just update the new image in via blhost and finally reboot.

Gavin_Jia_0-1719486616556.pngGavin_Jia_0-1719486616556.png

Execute the flashloader project in RAM and run the following command, which returns success, just to confirm that the flashloader has run successfully:

blhost.exe -p COM60 -- get-property 1

Finally, how to write the new image to flash via uart, you need to execute a lot of blhost commands, which are recorded by the software MCUXpresso Secure Provisioning Tool, you can use this software to execute it once, then record these commands, and then execute it by yourself in the command line terminal afterward, and the effect will be the same.

I attached the command recorded on my side for your reference.

 

Best regards,
Gavin

 
0 件の賞賛
返信