Arbitrary Length Math with a 56F8013

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arbitrary Length Math with a 56F8013

ソリューションへジャンプ
4,126件の閲覧回数
jag
Contributor IV
Hi,
for a program I'm doing I need to do some math with very large numbers.
Very large numbers means 64 bits (signed) variables.
Just to be clear: it is not my decision to use 64 bit variables.
The problem is, as I think you have understood, that the 56800/E can NOT use 64 bit variables, but "only" 32 bits.
So I need to split the 64 bit variable in 2 chucks of 32 bit each, and do the math (only + and - luckily) with these 32 bits chucks.
Now I'm wondering if exist some algorithm already implemented for the 56800/E that do this kind of math.
Or else I'll write it, but I've no uidea how to manage the overflow (and underflow) of the low chuck.

Thanks Bye Jack
タグ(1)
0 件の賞賛
返信
1 解決策
2,969件の閲覧回数
jag
Contributor IV
I reply to myself :smileytongue:.

The 56800/E core can do 64 bit addition and subtraction (cfr. pag. 5-29 of DSP 56800E Reference Manual).

So problem solved. Or at least I don't have to implement the algorithm myself.
Now I just have to search for the C function (or write the assembler routine in my C code).

Bye Jack

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,970件の閲覧回数
jag
Contributor IV
I reply to myself :smileytongue:.

The 56800/E core can do 64 bit addition and subtraction (cfr. pag. 5-29 of DSP 56800E Reference Manual).

So problem solved. Or at least I don't have to implement the algorithm myself.
Now I just have to search for the C function (or write the assembler routine in my C code).

Bye Jack
0 件の賞賛
返信