Allowable void% on MRF1K50N solder joint?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Allowable void% on MRF1K50N solder joint?

2,297 Views
joshterry
Contributor I

We are trying to attach our MRF1K50N transistors to copper carriers using reflow soldering and wanted to know if you had a recommended or max allowable void% of the joint, so we know how much we need to improve our process and at what point we can call it successful.

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
1 Reply

2,140 Views
LPP
NXP Employee
NXP Employee

Our general safe limit for maximum solder voiding specification is 25% total area voided max and no single void greater than 5%.

For thermal strained applications, for a decent solder mount void requirement under the flange is 40 mils "approximately round" max void area and no more than 15% total voided area. 40 mils can be replaced with a 3% max single void area and max 15% overall voiding.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------