Hello.
I'm using sja1105-tool to configure the Qbv scheduling with referring "Open Industrial Linux User Guide Release v0.2". But this guide doesn't include details of the tool (e.g. meanings of the parameters of each table such as mac-configuration-table or l2-forwarding-table, etc.). I also saw the man pages of sa1105-tool, I couldn't see the meaning of each parameter. Are there any good ways or materials to understand these?
As an example, on the user guide page 61, the guide says "The user can select whether the switch includes the VLAN tags in the egress packet or not." How can I select this option? Which parameters should be configured?
Thanks.
hi : How to you get the sja1105-tool ?