Adding tempsensor driver using Manage SDK Component will remove FreeRTOS drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding tempsensor driver using Manage SDK Component will remove FreeRTOS drivers

1,022 Views
Amal_Satheesan
Contributor I

Hello,
I am using MIMXRT1176AVM8A controller and FreeRTOS for my project. I need to measure the temperature of the controller, but when I try to add the driver for tempsensor it is removing the FreeRTOS drivers. 
How can I work with tempsensor without affecting my FreeRTOS.
I have attached screen shots for reference.
SDK version is 2.16

Amal_Satheesan_0-1729602213794.png

 

Capture1.PNGCapture2.PNG

0 Kudos
Reply
1 Reply

1,001 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Amal_Satheesan ,

Thanks for your interest in NXP MIMXRT series!

I used the freertos_hello_world_cm7 example demo in the SDK as a start, adding this component did not affect freertos:

Gavin_Jia_0-1729670665203.pngGavin_Jia_1-1729670705970.png

Also, this driver should only have one .h/.c files, you can also try to add them manually.

BR
Gavin

0 Kudos
Reply