Adding own actuator model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding own actuator model

1,493件の閲覧回数
igor_lumpus
Contributor I

We are trying to use the PT2000 simulator with Custom Actuator and having a the model described in a C# file.

When running the simulator it stops at first step (41 ns) without telling what went wrong.

This happens as soon any of the actuators is Custom with "FeedBack Source" set to External.

We have tried with very simple code and always end up with same result(or rather No result)

Is there any thing else we have to do in order to get the simulator running with the compiled actuator dll's?

タグ(3)
0 件の賞賛
返信
1 返信

1,439件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Igor,

I am not very familiar with this functionality, but I have forwarded this question to experts and hopefully will have an answer in a day or two.

It might be helpful if you could send us the simulator project. This would make it easier for us to debug it. If you are willing to do so, please create a standard private ticket.

Best regards,

Tomas 

0 件の賞賛
返信