Adding own actuator model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding own actuator model

1,489 Views
igor_lumpus
Contributor I

We are trying to use the PT2000 simulator with Custom Actuator and having a the model described in a C# file.

When running the simulator it stops at first step (41 ns) without telling what went wrong.

This happens as soon any of the actuators is Custom with "FeedBack Source" set to External.

We have tried with very simple code and always end up with same result(or rather No result)

Is there any thing else we have to do in order to get the simulator running with the compiled actuator dll's?

Tags (3)
0 Kudos
Reply
1 Reply

1,435 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Igor,

I am not very familiar with this functionality, but I have forwarded this question to experts and hopefully will have an answer in a day or two.

It might be helpful if you could send us the simulator project. This would make it easier for us to debug it. If you are willing to do so, please create a standard private ticket.

Best regards,

Tomas 

0 Kudos
Reply