Accessing SDK Wizard/installing additional drivers in MCUXpresso after initial project creation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing SDK Wizard/installing additional drivers in MCUXpresso after initial project creation

ソリューションへジャンプ
944件の閲覧回数
Tristian475
Contributor I

Is there a way to re-access the SDK Wizard after the initial time you configure a project? Basically, at that point it lets you select which drivers you want and includes them in a drivers folder. However, as time went on I found that I need to add more drivers than I originally planned for. How do I select additional drivers to incorporate from the SDK after initial project creation?

0 件の賞賛
返信
1 解決策
933件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

You can use Manage SDK components to add SDK drivers:

Alice_Yang_0-1646116501663.png

 

BR

Alice

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
934件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

You can use Manage SDK components to add SDK drivers:

Alice_Yang_0-1646116501663.png

 

BR

Alice

 

0 件の賞賛
返信
920件の閲覧回数
Tristian475
Contributor I

Yes thanks i got it.

0 件の賞賛
返信