Accessing SDK Wizard/installing additional drivers in MCUXpresso after initial project creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accessing SDK Wizard/installing additional drivers in MCUXpresso after initial project creation

Jump to solution
948 Views
Tristian475
Contributor I

Is there a way to re-access the SDK Wizard after the initial time you configure a project? Basically, at that point it lets you select which drivers you want and includes them in a drivers folder. However, as time went on I found that I need to add more drivers than I originally planned for. How do I select additional drivers to incorporate from the SDK after initial project creation?

0 Kudos
Reply
1 Solution
937 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

You can use Manage SDK components to add SDK drivers:

Alice_Yang_0-1646116501663.png

 

BR

Alice

 

View solution in original post

0 Kudos
Reply
2 Replies
938 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

You can use Manage SDK components to add SDK drivers:

Alice_Yang_0-1646116501663.png

 

BR

Alice

 

0 Kudos
Reply
924 Views
Tristian475
Contributor I

Yes thanks i got it.

0 Kudos
Reply