AFSC5G35D35 PA Performance for 5G Signals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AFSC5G35D35 PA Performance for 5G Signals

907 次查看
ibr
Contributor I

Hello

I need to know that typical performance of AFSC5G35D35 Power Amplifier is given for LTE signal, 1 x 20 MHz LTE, Input Signal PAR = 8 dB @ 0.01% Probability on CCDF, what will be performance of this device if tested under 5G OFDM signals with BW=100 MHz and PAR of 8-9dB?

For LTE output power is mentioned to be 3W average. I need to understand what will be the impact on output power when a signal with wider bandwidth like 5g is input to this device? Is there a relation of input signal BW with Output of device?

Thank you

0 项奖励
回复
0 回复数