AFSC5G35D35 PA Performance for 5G Signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFSC5G35D35 PA Performance for 5G Signals

914件の閲覧回数
ibr
Contributor I

Hello

I need to know that typical performance of AFSC5G35D35 Power Amplifier is given for LTE signal, 1 x 20 MHz LTE, Input Signal PAR = 8 dB @ 0.01% Probability on CCDF, what will be performance of this device if tested under 5G OFDM signals with BW=100 MHz and PAR of 8-9dB?

For LTE output power is mentioned to be 3W average. I need to understand what will be the impact on output power when a signal with wider bandwidth like 5g is input to this device? Is there a relation of input signal BW with Output of device?

Thank you

0 件の賞賛
返信
0 返答(返信)