AFM906N MET Model Parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFM906N MET Model Parameters

1,561件の閲覧回数
tberezowsky
Contributor I

Hello Everyone, 

I'm not sure the best location to post this question. Please let me know! :smileyhappy:

I'd like use the AFM906N in a design around 140MHz, but NXP is not providing data below 240MHz. In addition, I do not have ADS or AWS, but if NXP or anyone else could provide me with the MET model parameters for the AFM906N so I can simulate in alternative SW, it would be greatly appreciated. 


Lastly, does anyone know why NXP will provide a reference DXF but not a schematic? 

Thanks! 

Tyler 

タグ(2)
0 件の賞賛
返信
1 返信

1,502件の閲覧回数
tberezowsky
Contributor I

: ( Can I be given the S2P file at 140MHz? 

0 件の賞賛
返信