ADS model for BLS6G3135-20 LDMOS Transistor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADS model for BLS6G3135-20 LDMOS Transistor?

1,147 Views
bhagathsinghche
Contributor I

Hi,

I'm designing a multistage power amplifier using BLS6G3135-20 and BLS6G3135-120 LDMOS RF Transistors.

I am using Agilent ADS 2016 to simulate and generate the layout of the power amplifier. In order to simulate it, I need the ADS Models for these two transistors. However, the model files (for ADS 2009) which are shown on the website are not downloadable.

It will be of immense help to me if  anyone can provide me either with the Model Files for ADS or the S-parameter values

Thanks in advance.

Labels (1)
  • RF

0 Kudos
Reply
0 Replies