A2I20D040N DC Biasing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A2I20D040N DC Biasing

907 Views
chinhee
Contributor I

Hi,

I am a bit confused with the A2I20D040N power amplifier biasing. Hope that I can get some help here.

Can I connect Vgs1A and Vgs2A together?

Similarly, Can I connect Vds1A and VBWA together, leaving Vds2A unconnected to DC biasing? 

0 Kudos
Reply
1 Reply

891 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Chin,

I hope all is great with you.

As long as the parameters mentioned are with the specifications, the device might work as expected.

diazmarin09_0-1661891152188.png

 

In this case, I do recommend to review the circuit design from the RF Circuit Collection. You may use it as a reference for your design.

Have you considered using the S-parameter to simulate the device behavior? You may find such material and more at the link below:

A2I20D040N - 1400-2200 MHz, 5 W Avg., 28 V Wideband Integrated RF LDMOS Amplifier

I hope this information helps.

Regards,

David

0 Kudos
Reply