A1006 Authenticate IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A1006 Authenticate IC

1,861 Views
Dayanandkilledar
Contributor I

Hi All,

can anyone tell the sequence flow for the A1006 IC.

I was following the A1006 Secure Authenticator IC Product short data sheet

for example when can use the powerdown, wakeup, lockdevice, changeaddress, softreset and what is the sequence?

what is the minimum delay should i keep in between these API's.?
can anyone provide me the proper sequence flow of these API's.

0 Kudos
Reply
1 Reply

1,850 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Dayanandkilledar ,

 

Actually this part is a none mass market product and all its documents are under NDA, we are not allowed to share the info here publicly , and such kind of products are usually supported by NXP FAE, is there any FAE following up with your project?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply