A1006 Authenticate IC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A1006 Authenticate IC

1,857件の閲覧回数
Dayanandkilledar
Contributor I

Hi All,

can anyone tell the sequence flow for the A1006 IC.

I was following the A1006 Secure Authenticator IC Product short data sheet

for example when can use the powerdown, wakeup, lockdevice, changeaddress, softreset and what is the sequence?

what is the minimum delay should i keep in between these API's.?
can anyone provide me the proper sequence flow of these API's.

0 件の賞賛
返信
1 返信

1,846件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Dayanandkilledar ,

 

Actually this part is a none mass market product and all its documents are under NDA, we are not allowed to share the info here publicly , and such kind of products are usually supported by NXP FAE, is there any FAE following up with your project?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信