8306 Ram problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

8306 Ram problem

1,982 次查看
gnamba
Contributor I
hi sir,sorry for my bad english.!!!I have make a board design with mpc8306.this project isbased on evb of mp8306SOM.I have same flash chip and same ram (nand02gw3b2dza6e &mt47h64m16hr-3h), but it seems that we can't comunicatedwith this devices,for example i can't use the flash eraseprogram probably because  i have a problem with .cfg file orbecause i have another problem.i receive randomly this message:-Error: getting id failled-Error:  Couldn't write flash driver to target.  See Details foradditional informationi can write in register and, for example, pull up some GPIO. itseems that the tap comunication work properly but notthingelse.do you have any idea?you can help me please?you can send me a valid .cgf file or a guide to make it?

0 项奖励
回复
2 回复数

1,837 次查看
genuap
NXP Employee
NXP Employee

I'm assuming you're using codewarrior?

 

To burn the flash chip you actually need RAM available on the board. This is typically DDR. So, before you try and program flash work on getting your DDR up and running correctly. 

 

You can enter in settings for your particular DDR in the cfg file for codewarrior. You can then use the Hardware Diagnostics to test your DDR. This will run extensive memory tests on it.

 

 

Once you have DDR working, you need to tell the flash programmer where to find free buffer space - this is where you should put your DDR base address. 

 

 ... Paul

 

1,837 次查看
gnamba
Contributor I

thanks paul,

i try it..

0 项奖励
回复