74LVC2G125

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

74LVC2G125

2,657 Views
junboyi
Contributor I

The Data Sheet says:

This device is fully specified for partial power-down applications using IOFF. The IOFF circuitry
disables the output, preventing a damaging backflow current through the device when it is powered
down.

The similar device SN74LVC2G125 from TI says:

This device is fully specified for partial-power-down
applications using Ioff. The Ioff circuitry disables the
outputs, preventing damaging current backflow
through the device when it is powered down.

Ioff Supports Live Insertion, Partial-Power-Down
Mode, and Back-Drive Protection.

Partial Power Down (Ioff):
The inputs and outputs for this device enter a high impedance state when the supply voltage is 0 V.

Logically, NXP 74LVC2G125 is the same as TI SN74LVC2G125, 

but I would like to make sure whether the input is in high impedance or not while Vcc=0 for NXP 74LVC2G125. 

0 Kudos
Reply
1 Reply

2,576 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately 74LVC2G125 had already transfer into NEXPERIA,you can contact with them for more technical support!

74LVC2G125 - Dual bus buffer/line driver; 3-state | Nexperia 

0 Kudos
Reply