74LVC1G14 Part Input Leakage Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

74LVC1G14 Part Input Leakage Current

1,614件の閲覧回数
Santhosha_rk
Contributor I

Hi,

I was going through the datasheet of 74LVC1G14GW part, which reads the Input leakage current as +/-100uA for -40 to +125 degC part and +/-5uA max for -40 to +85 degC part (Page 5 of datasheet). This part comes only in -40 to +125 degC packaging. Is it not clear from the datasheet, so we assume that the leakage current would be limited to 5uA when the device is operated in the temperature range -40 to +85 degC. Please let me know if my assumption is correct, if not please let me know the maximum leakage current for the part?

Regards,

Santhosha RK

0 件の賞賛
返信
1 返信

1,520件の閲覧回数
LPP
NXP Employee
NXP Employee

The leakage current would be limited to 5uA when the device is operated in the temperature range -40 to +85 degC whereas it would be 100uA in wider temperature range.

0 件の賞賛
返信