16 Channel Adjustable Constant Current LED Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

16 Channel Adjustable Constant Current LED Driver

Jump to solution
2,388 Views
guitardenver
Contributor IV

I'm looking for a drop in replacement for the TI TLC5926IPWPR LED driver.

 

It's 16 channel constant current LED driver. Max current is set via an external resistor, but we can also adjust the current via the SPI interface.

 

Does NXP have this as well? I do not need error detection feature. Just need to adjust the current via SPI bus.

5mA to 61mA output current.

0 Kudos
Reply
1 Solution
2,347 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Matt,

There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.

The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:

https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf

There is a table with all NXP’s LED controllers available in the following document, page 3:

https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
2,348 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Matt,

There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.

The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:

https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf

There is a table with all NXP’s LED controllers available in the following document, page 3:

https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf

Best regards,

Tomas

0 Kudos
Reply