16 Channel Adjustable Constant Current LED Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

16 Channel Adjustable Constant Current LED Driver

ソリューションへジャンプ
2,418件の閲覧回数
guitardenver
Contributor IV

I'm looking for a drop in replacement for the TI TLC5926IPWPR LED driver.

 

It's 16 channel constant current LED driver. Max current is set via an external resistor, but we can also adjust the current via the SPI interface.

 

Does NXP have this as well? I do not need error detection feature. Just need to adjust the current via SPI bus.

5mA to 61mA output current.

0 件の賞賛
返信
1 解決策
2,377件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Matt,

There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.

The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:

https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf

There is a table with all NXP’s LED controllers available in the following document, page 3:

https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,378件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Matt,

There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.

The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:

https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf

There is a table with all NXP’s LED controllers available in the following document, page 3:

https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf

Best regards,

Tomas

0 件の賞賛
返信