UWB: Two-way ranging measurements with 0x21 status (Ranging RX timeout)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UWB: Two-way ranging measurements with 0x21 status (Ranging RX timeout)

1,942件の閲覧回数
ver-kapi
Contributor I

Hi,

I am in the process of porting the UWB middleware to the Zephyr-RTOS environment for my product needs. I can complete the UWB establishment procedure with the iOS peer over Bluetooth and initialize the UWB session. However, after I start ranging with the iOS peer, every UWB ranging measurement (two-way) contains invalid distance data (0xFF 0xFF) and the 0x21 status code, which maps to the RX ranging timeout.

Do you have any advice on what I might be missing in my project? Is there anything in particular that I should double-check for this particular issue?

0 件の賞賛
返信
1 返信

1,909件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. You are using a Module/Kit from one of our Trimension UWB Partners, right?

In that case, you would need to go directly with them to receive support for their Module/Kit.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

0 件の賞賛
返信