SR040 porting to ESP32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SR040 porting to ESP32

ソリューションへジャンプ
2,295件の閲覧回数
dtquang
Contributor I

Dear all, NXP team,

I am working on porting the NXP SR040 UWB library to ESP32.

I am facing an issue that the SPI transaction from ESP cannot read any data from the SR040. I am not sure whether the SPI on SR040 has any specific requirements. Looking from logic analyzer, the clock seems to stop right at first bit. I don't really have any idea.

If you have any experience with porting to ESP32, can you please give me some advice.

Thank you.

Best regards,

Quang

0 件の賞賛
返信
1 解決策
2,277件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Quang,

 

Hope you are doing well. Are you using one these Development Kits or Modules (UWB Developer Resources)? If that is the case, you would need to go directly with the Module Maker to know the process and the support that they can provide you.

 

Regards,

Ricardo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,278件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Quang,

 

Hope you are doing well. Are you using one these Development Kits or Modules (UWB Developer Resources)? If that is the case, you would need to go directly with the Module Maker to know the process and the support that they can provide you.

 

Regards,

Ricardo

0 件の賞賛
返信