Reg: UWB Related Queries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: UWB Related Queries

2,792件の閲覧回数
Rishikesh1
Contributor I

1. At what frequency do we have to change the battery cells in UWB Tag?

2. What is the range of UWB tags indoors?

3. How many antennas will be required for a 5000 sq feet area? (In the NXP demo video we saw 4 antennas are required for 100 sq feet. Out of the 4 antennae, one is acting as a master whereas the other 3 is acting as a slave).

4. How many slaves communicate with one master?

5. Can we transmit data using UWB? If yes means, how?

6. What will be the Cost of the UWB tag and UWB antenna?

0 件の賞賛
返信
3 返答(返信)

2,769件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

As some of the information of UWB is still under NDA and can't be disclosed in a public way such as this community  and in order to keep all the information in a single support line, is there a way that you can help using the internal case number you already submitted?

 

Regards

 

 

0 件の賞賛
返信

2,759件の閲覧回数
Rishikesh1
Contributor I

Hi 

I have already submitted the ticket.

Case Number: 00481460 

FYKI,

 

Rishikesh G

 

 

タグ(1)
0 件の賞賛
返信

2,751件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for the information , the case will be updated as soon as possible .

 

regards

0 件の賞賛
返信