NXP Trimensions AR app in Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Trimensions AR app in Android

2,235件の閲覧回数
hungli33
Contributor II

Dear Sir / Madam,

I am working on the SR150 solution and I can find a NI software to work with NXP Trimensions software thru iphone 12 or above but I don't sure is there any similar NXP Trimensions software running in Samsung S22+ or other Android having UWB chip inside.  If yes, can you share me APK file for trial?

タグ(2)
0 件の賞賛
返信
1 返信

2,194件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of these products it's under NDA (Non-Disclosure Agreement) the information it's not public, this is not a secure channel to share any information of this device and I do not have the data as well for the same reason.

If you are using one of the Development Kits or Modules from our Partners (Trimension UWB Partners), you would need to go directly with them to know the process and the support that they can provide you, as the support path for this technology is through them.

 

Hope this helps!

 

Regards,

Ricardo

0 件の賞賛
返信