Account setup and login method using vsftp (331,530 error)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Account setup and login method using vsftp (331,530 error)

2,748 Views
hsj
Contributor I

20240828_095653.png20240828_100224_1.jpg

 

20240828_100224_2.jpg

 

I only want to log in to the account with the password set in vsftpd.conf, so I set it as follows.

After setting up, when I enter the account and password set in the Filezila program, 331 and 530 errors occur.

The password has been tried in various formats, and the same problem occurs even if the password is entered correctly.

The linux kernel version is 6.1.22, and the vsftpd version is 3.0.5.
The architecture is arm64. (Operating System: NXP i.MX Release Distro 6.1-mickledore (mickledore))

The account was made with the "passwd ftp" command.

Is there a way to solve this problem?

0 Kudos
Reply
0 Replies