I have a USBDM that uses MC9S08JM60.Its USBDM version is 4.9.4 and Its hardware date is 2011/10/27.It works well.Now I want to debug Kinetis L series chip.So,I update the firmware to Version V4_10 and Install the USBDM_4_10_4a_Win.msi.But It doesn't work.I log in the community and find the new hardware in package version 4.10.0.Did you change the hardware? Can firmware V4_10 work on my USBDM board?
The Kinetis MKL series of devices only have a SWD interface. It is likely that the version of USBDM you have only supports the JTAG interface used on the MK devices.